{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number of a directory for an 84 circuit panel ?
Issue:
What is the part number of a directory for an 84 circuit  panel ?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker panelboards sold and supported in the USA.

Resolution:
Use a 80031-158-01 card for 1-42 and a 80031-158-02 card for 43-84 . These are also available on-line for computer keyboarding in 0120SM1001
( Horizontal layout) or 0120SM1008 ( Vertical ) .

Schneider Electric Canada

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: