{}

Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Where can I find a manual and ESI file for VW3A3601 EtherCAT Module?
Issue:
Manual and ESI file for Altivar drives using EtherCAT option card

Product Line:
ATV32
ATV320
ATV340
ATV900


Environment:
All

Cause:
EtherCAT Connectivity

Resolution:

The EtherCAT option card manuals are specific to each drive family they are being installed in.  See the following links:
ATV32: https://www.se.com/ww/en/download/document/S1A28703/
ATV320: https://www.se.com/ww/en/download/document/NVE41315/
ATV340: https://www.se.com/ww/en/download/document/NVE61686/
ATV900: https://www.se.com/ww/en/download/document/NHA80946/

The ESI files for the Module VW3A3601 are dependent on the version of the option card:
V1.01 (ATV32 only): https://www.se.com/ww/en/download/document/ATV32_EtherCAT_ESI/
V1.03 (ATV32 only)" https://www.se.com/ww/en/download/document/ATV32%20EtherCAT%20ESI%20file_V103/
V1.09 (Min FW version for ATV320): https://www.se.com/ww/en/download/document/EthCAT_VW3A3601_V109/
V1.12: https://www.se.com/ww/en/download/document/EthCAT_VW3A3601_V112/
V1.13: https://www.se.com/ww/en/download/document/EtherCAT_ESI_VW3A3601_V113/
V1.14: https://www.se.com/ww/en/download/document/EtherCAT_ESI_V1.14/

As additional versions are released the website will be update to include them.

Schneider Electric Česká republika

Zjistěte více
Produkt:
Řada:
Zjistěte více
Produkt:
Řada: