Vores varemærker

Impact-Company-Logo-English Black-01-177x54

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
Is there a NetShelter SX cabinet or rails available that support 21" wide EIA equipment mounting?
Issue:
Whereas EIA/ECA 310-E standard supports 19" and 23" wide equipment mounting, customers sometimes ask for 21".

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
We cannot find any information regarding NetShelter SX cabinets and a 21" rackmount standard.

Resolution:

The European Telecommunications Standards Institute  (ETSI) has 21-inch rackmount standard.
We do not currently offer cabinets made to the ETSI 21" standard, but if you have an opportunity with some quantity please contact APC Sales. The CustomRacks team may be able to quote this.