Issue:
There may be physical differences between the HS and SX models.
Product Line:
NetShelter SX and HS.
Environment:
All models, all serial numbers.
Cause:
Customers may want to make sure which accessories install into the new cabinet, and where.
Resolution:
The HS cabinet frame is higher to accommodate taller castors, but the inside dimension of the frame has not changed.
In the NetShelter SX there are some 0U mounting spaces behind the vertical rails of the frame. These don't exist on the NetShelter HS. (see attached)
There may be physical differences between the HS and SX models.
Product Line:
NetShelter SX and HS.
Environment:
All models, all serial numbers.
Cause:
Customers may want to make sure which accessories install into the new cabinet, and where.
Resolution:
The HS cabinet frame is higher to accommodate taller castors, but the inside dimension of the frame has not changed.
In the NetShelter SX there are some 0U mounting spaces behind the vertical rails of the frame. These don't exist on the NetShelter HS. (see attached)
Publié pour: Schneider Electric Algeria


Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.