Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
		
En quoi pouvons-nous vous aider aujourd'hui ?
How to activate Motor analog PTC in TeSys T (LTMR) using SoMove?

The PTC Analog motor temperature sensing function is enabled when the Motor Temp Sensor Type parameter is set to PTC Analog and the LTM R controller is connected to an analog PTC thermistor embedded in the motor.

1

The PTC analog motor temperature sensor function has the following configurable parameter settings:
Fault thresholds setting range 20....6500 ohms

2


Warning thresholds setting range 20....6500 ohms

3

However, this value needs to be set as per the motor/thermistor specifications.

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :
  • Documentation produit
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
  • Politique de confidentialité
  • Mention sur les cookies
  • Change your cookie settings