Issue:
External keypad option for E-Flex Nema 3R drive
Product Line:
Altivar Machines
Environment:
NEMA 3R only E-Flex drives
Cause:
Needs to order an NEMA 3R -E-Flex drive with a remote keypad display mounted on the door.
Resolution:
The E-Flex drive is obsolete. External keypad was not available on the E-Flex. The replacement ATV660 drive also does not have an option for external keypad on Nema 3R, as they are not UV protected.
External keypad option for E-Flex Nema 3R drive
Product Line:
Altivar Machines
Environment:
NEMA 3R only E-Flex drives
Cause:
Needs to order an NEMA 3R -E-Flex drive with a remote keypad display mounted on the door.
Resolution:
The E-Flex drive is obsolete. External keypad was not available on the E-Flex. The replacement ATV660 drive also does not have an option for external keypad on Nema 3R, as they are not UV protected.
Released for: Schneider Electric Egypt and North East Africa


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.