Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why are the Overload and On-Line LEDs flashing on my APC Back-UPS?
Issue:

Why are the Overload and On-Line LEDs flashing on my APC Back-UPS?


Product Line:

Back-UPS CS, Back-UPS PRO, Back-UPS USB, Back-UPS LS, Back-UPS NS/XS/RS


Environment:

Back-UPS CS, Back-UPS PRO, Back-UPS USB, Back-UPS LS, Back-UPS NS/XS/RS


Cause / Resolution:

When a Back-UPS UPS flashes the On-Line and Overload LEDs alternately, it is signifying that the unit is in ""Sleep"" mode after the optional shutdown software has gracefully shutdown the operating system. In this state the unit
turns off its output power to conserve the battery as the unit waits for normal input power to return. When power returns and is deemed safe for your equipment the UPS will then ""wake-up"" and turn back on its output power.
Normally, it is the optional shutdown software (PowerChute Personal Edition, PowerChute Business Edition) that commands the UPS to go to sleep once it has gracefully shutdown the operating system.
It is possible and normal, however, for the UPS under certain circumstances to go to sleep even though no optional shutdown software is being used in conjunction with the UPS. There are two possible scenarios that can cause the UPS to spontaneously go into ""Sleep"" mode.

1. If the UPS's battery is disconnected and reconnected while the UPS is operating On-Battery (4 beeps every 30 seconds, yellow On-Battery LED is illuminated) this will occur.


2. If the battery is disconnected while the unit is On-Line and then the UPS goes to battery (either because of a power problem or because the UPS's input power cord is unplugged) this will also occur.


Turning the unit off and back on with the battery connected will clear this symptom.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings