Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Telephone/DSL Splitter of the S15 & S15BLK, AV Power Conditioner w/ Battery Backup.
Issue:

The S15, Power Conditioner with Battery Backup has a Telephone/DSL line splitter, along with COAX and Ethernet surge protection

Product Line:

S-Type Power Conditioner w/ Battery Back-up.

Environment:

S15, S15BLK

Cause / Resolution:

The Telephone/DSL splitter will accept a 2-line 4-wire telephone connection and splits it off into two separate telephone lines. When a telephone connection comprised of two separate telephone lines, is connected to the Telephone/DSL splitter, line ONE will be split to ""Out A""(pins 2&3) and line TWO will be split to ""Out B""(pins 2&3).

The Telephone/DSL splitter DOES NOT split a single 1-line 2-wire connection.

Note:
On a standard telephone connection, a customer can have a maximum of two separate telephone lines/numbers. Line ONE is between (pins 2&3) of the RJ-11 connection. Line TWO (this only applies to customers who have requested a second line from the telephone company) would be between (pins 1&4).&

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings