Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What's the difference between ATV312 & ATV71 in the same power rating?
There are certain differences between the ATV71 & the ATV312:

The ATV71 has the following differences:

1. Wider output frequency range ( 0.1 -1600 Hz ).

2. It can drive asynchronous & synchronous motor, unlike the ATV312 which drives asynchronous motors only.

3. It can withstand a transient torque up to 220% of the nominal torque.

4. it has more than 150 functions, unlike the ATV312 which has 50 functions.

5. It has more analogue & logic I/Ps and O/Ps, with an extra safety input.

6. It can come with an integrated DC choke.

But. performance-wise, both are the same.