Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to automatically start ProWORX 32 with a project from a command line

Issue
How to automatically start 'ProWORX 32' with a project.from a command line.

Product Line
ProWORX 32 version 2.1, SP2

Environment
Windows 10

Resolution
A Shortcut pointing to the '.pwx. file for the project can be used to automatically open ProWORX 32. The target path name for the shortcut can then be used as a DOS command to open the project.




Before the shortcut will work, the '.pwx' file must be associated to the Windows Registry. To associate the .pwx file, use the following steps.

  • Open the 'ProWORX\32\Projects' folder.
  • Double click on any '.pwx' file.

  • Click on the check box next to 'Select the program from a list'
  • Click on 'OK' to open the 'Open With' window.
  • Click on 'Browse' button and browse for the '.pwx' file.
  • Click on the check box next to 'Always use the selected program to open this kind of file' in the 'Open With' window.
  • Click on OK.


.Note: This feature will only work on 'ProWORX 32 version 2.1, SP2' and later versions.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings