Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do ION Meters support "Classless IP addressing"?

Issue
Classless IP addressing means that the IP address and the SUBNET mask of the device can belong to different classes.
There are three classes of IP addresses: A, B, and C. Each class covers a different of the range of the first octet of the IP Addresses:

Class A: 1-126

Class B: 128-191

Class C: 192-223

For example, 192.168.1.1 is a class C  and 126.168.68.10 is class A IP address.

The classes for the Subnet mask is a little different. The classes are as follows:

Class A: 255.0.0.0

Class B: 255.255.0.0

Class C: 255.255.255.0

It is possible to use a Subnet that is greater than the minimum values listed above. However, it would be inconsistent to use a Subnet lower than those values.


Below are examples of appropriate and inappropriate examples of IP/Subnet pairs:

Right: IP 10.168.68.10 Subnet 255.0.0.0

Right: IP 10.168.68.10 Subnet 255.255.248.0

Wrong: IP 192.168.1.1 Subnet 255.0.0.0

Product Line
ION Meters

Environment
IP Addressing

Resolution
ION Meters support classless IP addressing.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings