Issue
How do I perform basic communications troubleshooting steps on Powerlogic devices with Modbus communications?
Product Line
Powerlogic devices
CM2000, CM3000, CM4000, PM800, PM700, PM5000
EGX-100, 200, 300, 400
Environment
Energy monitoring
Cause
A PowerLogic device is experiencing communications problems and will require troubleshooting.
Resolution
1. If using an EGX or ECC card
Ping the EGX/ECC card IP address
If unable to ping: How to determine the IP address
If able to ping: Access the Webpage and write down the communication parameters (Baud rate, parity).
2. Check device list on the webpage and make sure that the device that is not communicating is in the list with the correct Device ID
3. Check DIP switches on the EGX/ECC card (see EGX/ECC installation manual )
4. Check the baud rate and parity on the serial device and make sure it matches the settings on the gateway
5. Check Device ID and make sure there are no duplicate IDs in the serial chain
6. Check Device wiring. The wiring from the master to first slave device follows: transmit goes to receive, receive goes to transmit.
7. Are wires installed to the serial port and not some other port such as the Digital input or KYZ pulsing if available?
8. At any point were wires other than communications wiring applied to the serial port?
9. Check the communication port and make sure that the Transmit ports measures around 5 volts. If the meter does not read any voltage then make sure the connector is plug in correctly. If it is, then the port might be damaged and the meter needs to be replace
Released for: Schneider Electric Egypt and North East Africa










Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.