Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can cable management arms such as AR8129 be used in NetShelter CX cabinets?

Issue:
There's not much space behind the rails in a NetShelter CX, and some U-spaces near the fans have no room.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
A customer wants to install the cable management arm into a NetShelter CX cabinet.

Resolution:

The space behind the rear mounting rails in the NetShelter CX cabinets should be left open as much as possible to allow proper airflow. Cable management arms can be used but must be confined to specific U-spaces so they don’t interfere with the fan modules.
Also, if the cable entry channel is being used care should be taken when installing AR8129 in the lower U-spaces.

• In the AR4018A or AR4018IA the AR8129 can only be mounted in U-spaces 1 through 7, and 12 through 18.

• In the AR4024A or 4024IA the AR8129 can only be mounted in U-spaces 1 through 6, and 12 through 20.

• In the AR4038A and AR4038IA the AR8129 can only be mounted into U-spaces 1 through 6, 12 through 20, 25 through 32 and 37 & 38.

See attachment below for illustration.

Schneider Electric Egypt and North East Africa

Attachment(s)
20140703 Mounting Behind the Rear Rail of NetShelter CX Cabinets.pdf [105.28 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings