Issue:
Information regarding the maximum load rating for the roof is required
Product Line:
NetShelter SX, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The load rating should not be exceeded.
Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.
Information regarding the maximum load rating for the roof is required
Product Line:
NetShelter SX, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The load rating should not be exceeded.
Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.
Released for: Schneider Electric Egypt and North East Africa




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.