Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the NetShelter WX castor kit AR8359 fit onto the AR106, AR109 or AR112.
Issue:
There doesn't appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
There is a request to add castors to AR106, AR109, AR112, AR106SH4, AR109SH4, AR112SH4, AR106SH6, AR109SH6, AR112SH6, AR106V or AR106VI.

Resolution:
There is no castor kit for the AR106, AR109 or AR112.
The smallest cabinet that has a castor kit available is the AR100  and AR100HD. They use AR8359 available as a castor kit.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings