Issue:
Using Coaxial cable with STO.
Product Line:
ATV61, ATV71, Altivar 61, Altivar 71
Environment:
All
Cause:
N/A
Resolution:
Yes, coaxial shielded cable is a must due to safety rules.
Explanation:
When we use STO only, the coaxial shielded cable is mandatory to be SIL2.
Because we use only one channel (no signal redundancy), in case of cable crushing:
• the shielded cable will put the signal to 0 and so, no safety issue
• When you have coaxial cable, no risk to have another potential to the STO, via another cable on same conduit
If you do not have shielded and coaxial cable, you have the risk to not detect the cable crushing and consequently not detect a safety stop.
So here, a shield is mandatory to reach the safety level and avoid safety issue on the machine.
Using Coaxial cable with STO.
Product Line:
ATV61, ATV71, Altivar 61, Altivar 71
Environment:
All
Cause:
N/A
Resolution:
Yes, coaxial shielded cable is a must due to safety rules.
Explanation:
When we use STO only, the coaxial shielded cable is mandatory to be SIL2.
Because we use only one channel (no signal redundancy), in case of cable crushing:
• the shielded cable will put the signal to 0 and so, no safety issue
• When you have coaxial cable, no risk to have another potential to the STO, via another cable on same conduit
If you do not have shielded and coaxial cable, you have the risk to not detect the cable crushing and consequently not detect a safety stop.
So here, a shield is mandatory to reach the safety level and avoid safety issue on the machine.
Released for: Schneider Electric Egypt and North East Africa




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.