The IP address can be read by using explicit command Read_Var.
In the ADDM the address would be 'r.m.c.server address'
Here r is rack number, m is module slot of ENOC module, c is channel & server address is "100".
So the syntax would '0.3.0.100' where 3 is module slot and 100 is server address in the ENOC module.
Now to read the IP address the modbus data mapping is as follow : Address 40006 (IP1 & IP2) and Address 40007 (IP3 & IP4) :

In the ADDM the address would be 'r.m.c.server address'
Here r is rack number, m is module slot of ENOC module, c is channel & server address is "100".
So the syntax would '0.3.0.100' where 3 is module slot and 100 is server address in the ENOC module.
Now to read the IP address the modbus data mapping is as follow : Address 40006 (IP1 & IP2) and Address 40007 (IP3 & IP4) :
Released for: Schneider Electric Egypt and North East Africa






Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.