Issue:
With the the ATV320, the manual states that bLF (Brake Logic Fault) can be reset by a logic input, but appears this does not work?
Product Line:
ATV320
Environment:
Brake Logic Fault
Cause:
n/a
Resolution:
France response: That is correct, on actual ATV320 version BLF can be reset by power cycle or product reset (RP or RPA).
It is not possible to reset this fault with automatic reset or standard reset fault RSF.
Evolution request is already registered on this point (PEP0324717R). Today, it is planned to have this change on maintenance version of ATV320 for end of 2017. I do not have more precise date for this release.
In the meantime, a workaround for you would be to reset BLF by a logic input, you can use the RPA function. This function will manage a product reset via a logic input and will reset the BLF.
With the the ATV320, the manual states that bLF (Brake Logic Fault) can be reset by a logic input, but appears this does not work?
Product Line:
ATV320
Environment:
Brake Logic Fault
Cause:
n/a
Resolution:
France response: That is correct, on actual ATV320 version BLF can be reset by power cycle or product reset (RP or RPA).
It is not possible to reset this fault with automatic reset or standard reset fault RSF.
Evolution request is already registered on this point (PEP0324717R). Today, it is planned to have this change on maintenance version of ATV320 for end of 2017. I do not have more precise date for this release.
In the meantime, a workaround for you would be to reset BLF by a logic input, you can use the RPA function. This function will manage a product reset via a logic input and will reset the BLF.
Released for: Schneider Electric Egypt and North East Africa


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.