Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerChute Network Shutdown v4.x fails to shutdown the vCenter Server VM or ESXi hosts when using a local account.

Issue:
PowerChute Network Shutdown v4.x fails to shut down the vCenter Server VM or ESXi hosts when using a local account.

This issue manifests itself as follows when attempting to shut down ESXi hosts during a shutdown sequence, as seen in the PowerChute error log.

19-05-18 10:44:38,096 ERROR Thread-40 com.apcc.m11.components.WebServer.util.virtualization.VMWareConnection - Unable to log directly into host (NoPermission or InvalidLogin): 192.168.1.10

19-05-18 10:44:38,096 DEBUG Thread-40 com.apcc.m11.components.WebServer.util.virtualization.VMWareConnection - com.vmware.vim25.InvalidLogin


Product Line:
PowerChute Network Shutdown versions 4.x

Environment:
All support OS configured with VMware vCenter Server and ESXi host(s).

Cause:
PowerChute attempts to log in with a lower-case username
e.g.
User created in ESXi host and entered in PowerChute as PCNSUSER
When PowerChute contacts the host, it enters pcnsuser
The user is rejected because the ESXi host expects PCNSUSER (all uppercase letters).

Solution:
1 - Create a user in the host/s with lowercase letters.
2 - To avoid having to use a lowercase username, set the default SSO domain to localos.
Example: if using PCNSuser@localos set the default domain in vCenter to localos. This allows for connection to vCenter using the username "PCNSuser" without having to include "@localos" and use this in the PCNS UI. This would avoid PCNS converting the username to lowercase.
The same would be true for vsphere.local accounts - whatever the default domain is set to, you can use the username without having to include the domain name, "@vsphere.local".


Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings