As far as motor parameters allows you to configure motor rated parameters, e.g. nominal synchronous current, speed, etc. then you can use ATV even for smaller motor.
List of motors that appear in main screen for selected ATV size represents a kind of templates, so if you choose one of motors from the list, motor data will be ready to match that motor. But no problem to change these motor parameters manually. The best practice is to create one ATV configuration offline with smaller ATV320 (that matches BMP070) and to check which parameters are preconfigured for your motor. The same values then should be put into your real ATV320U22N4B
List of motors that appear in main screen for selected ATV size represents a kind of templates, so if you choose one of motors from the list, motor data will be ready to match that motor. But no problem to change these motor parameters manually. The best practice is to create one ATV configuration offline with smaller ATV320 (that matches BMP070) and to check which parameters are preconfigured for your motor. The same values then should be put into your real ATV320U22N4B
Released for: Schneider Electric Egypt and North East Africa


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.