In EcoStruxure Building Operation "EBO" Server Modbus TCP network/device basic properties, "Multiple queries" means that a number of queries will be sent out at the same time. The system will wait for those responses. If this option is disabled, the system will send one query and the wait for a response. "Multiple queries" is only supported on some Modbus devices, so make sure that the integrated Modbus device supports this option before enabling it. "Multi queries" can be enabled/disabled at the Modbus TCP network or device level.
Released for: Schneider Electric Egypt and North East Africa




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.