Issue
The PowerView display of SURT 15/20kVA UPS shows the status of a Pack 0 in the Batteries menu.
Product Line
Smart-UPS 15/20kVA
Environment
Cause
Pack 0 represents the global battery status if the system is using non-APC batteries in the UX configuration.
In a non-UX configuration, the Pack 0 status screen will still be available on the PowerView display even if the system has only APC battery packs connected. However, Pack 01 represents the 1st APC battery cabinet connected to the UPS, Pack 02 the 2nd APC battery cabinet, and so on.
Resolution
If using APC batteries, the values reported for Pack 0 can be ignored.
The PowerView display of SURT 15/20kVA UPS shows the status of a Pack 0 in the Batteries menu.
Product Line
Smart-UPS 15/20kVA
Environment
- Smart-UPS 15/20kVA All Models
- SURT192RMXLBP2
Cause
Pack 0 represents the global battery status if the system is using non-APC batteries in the UX configuration.
In a non-UX configuration, the Pack 0 status screen will still be available on the PowerView display even if the system has only APC battery packs connected. However, Pack 01 represents the 1st APC battery cabinet connected to the UPS, Pack 02 the 2nd APC battery cabinet, and so on.
Resolution
If using APC batteries, the values reported for Pack 0 can be ignored.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.