Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Attempts to repair a Control Expert license running in a virtual machine fails.
Issue
Attempts to repair a Control Expert license running in a virtual machine fails.

Product Line
Control Expert 14.

Environment
Windows 10, Windows 7

Resolution
Attempts to repair a Control Expert license that becomes untrusted after moving the VM to another host PC, fails. and the following
message is returned.

10-28-2019,14:15:24:626,ActBrick,ERR,2316, 9424,Response Action (Deny): Repair Deny, FulfillmentId: FID_17f6002f_16999dd36ed_4060,
Reason: 7581; Request includes a license that got untrusted and cannot be repaired. In case you are working on a virtual machine, it is not allowed
for copy protection reasons to clone a virtual machine that includes licenses. A-XXXX-XXXX-XXXX Solution: Please return your license
from the original virtual

This works as designed.  The Control Expert 14 license cannot be repaired if it is installed in a virtual machine.  To resolve the issue, the
license must be returned from the original VM running on the host PC that was used to activate it.  It can then be activated in the virtual machine
running on the new host PC.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings