Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION900, PM8000, ION7400 meter v3.0.0 firmware and ION Setup considerations

Issue
Considerations when using ION setup with V3.0.0 Firmware on ION900, PM8000, and ION7400 meters

Product
ION Setup
ION9000, ION7400, PM8000

Environment
ION9000, ION7400, or PM8000 meter with v3.0.0 firmware

Cause
Changes to the security in v3.0.0 firmware for HEP meters makes old versions of ION Setup not work

Resolution

Recommend a minimum version of ION Setup V3.2.20218.01 when interacting with HEP meters with v3.0.0 firmware.

When trying to load a standard security file, .scf, on a v3.0.0 HEP meter, ION Setup will display the following message

ION Setup warning to indicate that V3.0.0 meters will only support advanced security.
Firmware only supports Advanced Security but can still support a single Standard Login

Selecting Yes will disable the (Legacy Security Support), selecting No will enable (LSS).

Q: With advanced security, is the user name case sensitive ?
A: No, the user name is not case sensitive however certain options are not accepted; USER01, USER 01, USER 1, USER00001

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings