Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Upgrading an ION meter via ION over Modbus with ION meter as Modbus gateway fails

Issue
Unable to upgrade ION meter using ION over Modbus when an ION9000 or PM8000 or ION7400 meter is the Modbus gateway device

Product
ION9000
PM8000
ION7400

Environment
ION9000, PM8000, ION7400 is configured as Modbus gateway with ION meter downstream using ION over Modbus

Resolution
Workaround options at this time
A) Connect directly to the meter, ideally via Ethernet port
B) Use a different gateway device such as PAS, Com'X or EGX. Do not recommend upgrading meter firmware via serial connection when using ION over Modbus.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings