Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why does my CSH2 battery state of charge change with the load turned off, or no load connected?
Issue: Why does my CSH2 battery state of charge change with the load turned off, or no load connected?

Product Line: CSH2 Smart-UPS Charge Mobile Battery for Microsoft Surface Hub 2

Environment: all models, all serial numbers

Cause: If the CSH2 is disconnected from AC input, and the 24V DC output is turned on, the battery will discharge even if there is no load connected to the CSH2, or if the connected Microsoft Surface Hub 2 is turned off. The expected runtime with the CSH2 on 100% state of charge, 24 V DC output on, no load, on battery (AC input disconnected), is 43 hours.

Resolution: To avoid discharging the CSH2 battery while the load is turned off for an extended period, it is recommended to leave the CSH2 connected to AC input, or to turn off the 24 V DC output.

 

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: