Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Smart-UPS On-Line with Li-Ion batteries reports "Error B.08" or inaccurate runtime
Issue: Smart-UPS On-Line with Li-Ion batteries reports "Error B.08", or shows  inaccurate runtime remaining on the UPS LCD display, when XBP48RM2U-LI battery pack is connected.

Error B.08

Product Line: SRTL1000RM4UXLI, SRTL1000RM4UXLI-NC, SRTL1500RM4UXLI, SRTL1500RM4UXLI-NC, SRTL1000RMXLI, SRTL1000RMXLI-NC, SRTL1500RMXLI, SRTL1500RMXLI-NC, SRTL2200RM4UXLI, SRTL2200RM4UXLI-NC, SRTL3000RM4UXLI​​​​​, SRTL3000RM4UXLI-NC, SRTL2200RMXLI, SRTL2200RMXLI-NC, SRTL3000RMXLI, SRTL3000RMXLI-NC

Resolution: This is addressed in UPS firmware version 15.3. 

Restart the UPS, then update the UPS firmware to the latest version. Refer to FA16473FA279197 ​​​​​​​or FA170679 to update the UPS firmware.

 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: