arrow2_left Main Page arrow2_right Wiser KNX
thumbnail

Wiser KNX

Smarter, greener, better. Wiser KNX.

A brand new, completely redesigned mobile app for your Wiser for KNX controller, offering the ultimate in comfort and convenience. The Wiser KNX App allows you to control and monitor your home at anytime from anywhere!

Room-by-room control.
Control your lights, blinds, thermostat, AC, sockets, or any other KNX device in each room of your house. Select the ones you use the most to be displayed in your favorites for a quick access or if you prefer, assign schedules so that they are automatically triggered in the selected date or time.

Moments.
Create the perfect ambiance for any occasion. A dinner date at your house? A movie night? Just create a Moment that suits your needs, select which devices should be part of it, and assign them a default status. From now on, with the touch of a finger you can trigger that Moment.

Notifications.
For some critical events like water, gas, or smoke detection, your will get immediately notified to your smartphone. You can also access your notifications history through your in-app Message Center.

Voice control.
You can easily regulate and control your devices with a voice command via Amazon Alexa and Google Assistant.

…and this is just the beginning, we will periodically release new updates with new functionality.

Requirements:
  • Having a Wiser for KNX controller hardware version 2.0 or higher with internet connection.
  • Having installed Firmware 2.8.0 or higher and enabled the Cloud Connector and KNX IoT 3rd party API.
  • Having your Touch 3 visualization created. Those Rooms and Widgets are the ones visualized in the new Wiser KNX App.
IMPORTANT: If you have an existing account in the previous Wiser for KNX App, you MUST use the same account to log in to the new Wiser KNX App. You won't be able to register and pair the controller again.

Close

action_close

Also Available on...

Size iOS: 53,1 MB / Android: 17 MB
Price Free
Languages English , French, German,Italian Spanish, Swedish

Scan QR codes with your phone