Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

SoMove, free licence setup software, for PCs designed to configure Schneider Electric's motor control device

SOMOVE_FDT

SoMove_FDT is user-friendly setup software.
SoMove makes it easy to configure motor control devices from Schneider Electric.
SoMove can be launched several times to commission several devices simultaneously.
Easy to connect
Incorporates various functions such as configuration preparation, testing and start-up,and maintenance.

Need more information? Check our technical FAQs!

Easily find answers to the most frequently asked questions.