ABUS Crane Systems: Customer Story Key Figures
Energy savings of up to 40%
Larger quantities with high quality
Reduced downtime
Leading crane builder uses EcoStruxure Machine to develop intelligent, modular crane control system.
Discover EcoStruxure
Learn how your business can achieve success with EcoStruxure: Innovation at Every Level.
The Challenge
ABUS Crane Systems is one of the leading manufacturers of crane systems in Europe. Every year, it produces more than 5,000 cranes in 50 different versions, supplies more than 35,000 customers in Germany, and exports to 55 countries around the world.
• One size does not fit all where cranes are concerned, however, and each crane that ABUS builds differs in design, size, number of drives, and functions.
• To be competitive and meet their customers’ demands, ABUS faced:
• Numerous requirements for highly complex and customized crane systems
• The need to standardize modules to achieve shortest production time possible
• The ability to operate quickly, independent of time zones and location, by leveraging advancements like digital data processing for preventive maintenance and repair
The Solution
Apps, Analytics & Services: ABUControl intelligent crane control, expert delivery services
Edge Control: Modicon M221, M241, M251 controllers, XPSMC safety controller, EcoStruxure Machine Expert (formerly known as SoMachine and SoMachine Motion)
Connected Products: Altivar drives, Altivar power regeneration, Phaseo ABL power supplies, TeSys motor-protective circuit-breakers & contactors, OsiSense sensors, XU photoelectric switches, XS inductive encoders
• EcoStruxure Machine: The breadth of the portfolio can address all the needs of ABUS’ customers. It also serves as the foundation for further exploiting the potential of the IIoT in ABUS’ cranes.
• Hoisting expertise and collaboration at all stages: From drafting requirements, concept development, and proposing innovative solutions with new functionalities and features, to programming, testing, and final validation
• The result: ABUControl, an intelligent modular crane control system based on EcoStruxure Machine. All required crane functions can be implemented with just two standard modules - from simple to complex crane architectures, with several cranes and hoists. Machine options do not have to be programmed, and the system parameters are set up quickly and easily in the crane control software.
The Results
• Efficient and fast series production, and larger quantities with high quality
• Faster handling of crane production due to the standard implementation of all required crane functions using only two standard modules
• Faster and more flexible new development - faster response to customer needs
• Comfort and safety
• Higher crane availability - reduced downtime
• Energy savings of up to 40%
The Modicon M241 control solution, together with networked frequency inverters, deliver added safety and convenience and reduce crane system downtime. With the regenerative unit of Altivar drives, energy generated during braking can be fed back into the grid, enabling energy savings of up to 40%.
Digitization: The further development of networked solutions and the collection and utilization of data are the gateway to the IIoT, helping ABUS to open up additional opportunities – such as predictive maintenance and global service capabilities – to expand their business.
Schneider Electric's solutions have helped ABUS become more competitive. Thanks to this cooperation, ABUS is introducing new and innovative hoisting developments that increase crane availability and enable targeted maintenance measures worldwide.
Learn more
Access more customer stories
Don’t stop here. We’ve got lots of success stories to browse through.
Read moreDiscover EcoStruxure
Learn how your business can achieve success too.
Explore moreInnovation Summits
See highlights from recent Innovation Summits and find out about the next event.
Find out more
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.