Issue
What are the recommended Panel Server models for legacy products substitution?
_____________________________________________________________
Product Line
Panel Servers, PAS400, PAS600, PAS800
_____________________________________________________________
Environment
Legacy Gateways
_____________________________________________________________
Solution
The 3 models of EcoStruxure Panel Server are Universal (PAS600 series), Advanced (PAS800 series), and Entry (PAS400) that are recommended for legacy products substitution based on their functionalities and applications.
The recommended Panel Server models are listed as table below:
Entry (PAS400)
Universal (PAS600 series)
Advanced (PAS800 series)

Note: SmartLink SIB has additional features that can be replaced by Universal Panel Server (PAS600) connected with SmartLink Modbus (A9XMSB11).
Devices PAS600 and A9XMSB11 together cover most of the features that SmartLink SIB supports.
What are the recommended Panel Server models for legacy products substitution?
_____________________________________________________________
Product Line
Panel Servers, PAS400, PAS600, PAS800
_____________________________________________________________
Environment
Legacy Gateways
_____________________________________________________________
Solution
The 3 models of EcoStruxure Panel Server are Universal (PAS600 series), Advanced (PAS800 series), and Entry (PAS400) that are recommended for legacy products substitution based on their functionalities and applications.
The recommended Panel Server models are listed as table below:
Entry (PAS400)
Universal (PAS600 series)
Advanced (PAS800 series)
Note: SmartLink SIB has additional features that can be replaced by Universal Panel Server (PAS600) connected with SmartLink Modbus (A9XMSB11).
Devices PAS600 and A9XMSB11 together cover most of the features that SmartLink SIB supports.
Publicado para: Schneider Electric España
¿Necesitas ayuda?
Selector de productos
Encuentra rápida y fácilmente los productos y accesorios adecuados para tus aplicaciones.
Pedir presupuesto
Comienza tu consulta de ventas en línea y un experto se pondrá en contacto contigo.
¿Dónde comprar?
Encuentra fácilmente el distribuidor de Schneider Electric más cercano a ti.
Centro de ayuda
Encuentra recursos de soporte para todas tus necesidades en un solo lugar.