Schneider Electric offers beautifully designed glass panels with an intuitive touch interface to enable guests to control room temperature, lighting, curtains, services, and more for a best-in-class guest experience. Our complete line of Glass Touch Panels (GTP) is highly customizable to reflect each hotel’s unique visual aesthetic. The panels are EcoStruxure™ ready devices and integrate with the SpaceLogic RP-C Pro Room Controller through the Modbus RTU (RS485) serial interface.
Fichiers
Nom du fichier | ||
QGH7885600-4_SL-GTP-Modbus-LSSM-Installation-Instructions_EN_RH20231124.pdf
|
|
Produits associés
Gamme(s)/Produit(s)