Schneider Electric offers beautifully designed glass panels with an intuitive touch interface to enable guests to control room temperature, lighting, curtains, services, and more for a best-in-class guest experience. Our complete line of Glass Touch Panels (GTP) is highly customizable to reflect each hotel’s unique visual aesthetic. The panels are EcoStruxure™ ready devices and integrate with the SpaceLogic RP-C Pro Room Controller through the Modbus RTU (RS485) serial interface.
File
Nama file | ||
998-22355857-2_SL-GTP-Modbus-LSSM-Specification-Sheet_A4_EN_RH20231102.pdf
|
|
Produk terkait
Rentang produk: