FAQ Pencarian
Can you use an ATS48 soft starter for a resistive load?
Issue:
Can an Altistart ATS48 soft start be used for a resistive load?
Product Line:
ATS48
Environment:
Resistive Load
Cause:
n/a
Resolution:
No. The ATS48 soft starters can not be used with resistive loads. They require a lagging power factor. Soft starters are designed for motor loads only.
Can an Altistart ATS48 soft start be used for a resistive load?
Product Line:
ATS48
Environment:
Resistive Load
Cause:
n/a
Resolution:
No. The ATS48 soft starters can not be used with resistive loads. They require a lagging power factor. Soft starters are designed for motor loads only.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: