FAQ Pencarian
MGE EPS; documentation regarding VRLA battery storage
Issue:
MGE EPS; documentation regarding VRLA battery storage
MGE EPS; documentation regarding VRLA battery storage
Product line:
EPS/ Batteries
Environment:
All models, all serial numbers
Cause:
Documentation regarding VRLA battery storage that are used in the MGE EPS product line. However, most manufacturers have the same policy.
Resolution:
Shelf life is 6 months at 77F. This is assuming the batteries were fully charged when shipped.
Storing batteries at temps above 77F will require more frequent boosting. This is pretty much the industry standard for these larger VRLAs.
C&D Policy:
GNB Exide Policy:
Enersys Policy:
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: