FAQ Pencarian
What would cause the PRG characters to flash on the central display of a TSX 37 Micro?
The 'write protect switch' set in the 'write authorized' position will cause the PRG characters to flash on the central display of a TSX Micro.
Note: The TSX37 is obsolete and it is recommended to upgrade to the M340 with the x80 I/O contact locals Schneider Sales office or Distributor for more information.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: