FAQ Pencarian
How do we determine the maximum point of encoder ?
Goals and Symptoms
How do we determine the maximum point of encoder ?
Facts and Changes
ATV71
Codeur
Encoder
Causes and Fixes
Fmax = 300 Khz
Maximum point of encoder = 5000
The formule is :
Encodeur point = 1/rpm x Fmax x 60, rpm is the speed of the motor.
Example : Motor 50Hz 2830 tr/mn using at 110Hz then 6226 tr/mn
The calcul done = 2891 it must take a 2048 point
Legacy KB System (APS) Data: RESL173103 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 71
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: