Issue
The purpose of this resolution is to inform users of Momentum PRODUCTS that an error exists in the processor specifications of the Distributed I/O and Control Modicon Momentum flexible system for distributed I/O and control catalog, part number DIA6ED1040904EN, published 3/2005.
In the 'Selection Guide' on page 8, the description for the M1E Processor Adapters, as shown in the following, is incorrect:
Product Line
Momentum
Environment
Resolution
The following table is the correct description of the M1E Processor Adapter model numbers.
Diterbitkan untuk: Schneider Electric Indonesia