FAQ Pencarian
BMXNOC0401 Explicit Messaging CIP Modbus Object Read Example
Issue
The attached document is a CIP Modbus Object Read example for a BMXNOC0401 using the DATA_EXCH block to read from a Quantum 140NOC77101.
Product Line
140NOC77101
BMXNOC0401
TSXETC101
Resolution
This program will read from located registers in Schneider PLC's with the following network modules installed.
See attachment.
This program example does not apply to read located registers in Schneider PLC's through the following network module:
140NOC78000
Diterbitkan untuk:Schneider Electric Indonesia
Lampiran
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: