FAQ Pencarian
What is the part number for the replacement battery on a ION7550 or ION7650? Can this be ordered?
Issue
What is the part number for the a battery replacement on the ION7X50
Product Line
ION7650
ION7550
ION7600
ION7500
Environment
Product Selection
Resolution
Schneider Electric no longer sells replacement batteries for the ION 7550 and ION 7650 because the batteries are now soldered to the board. For older versions of the meter, the battery can be replaced with a "Tadiran Model: TL-5276/W or equivalent". Please follow the attached document for battery replacement instructions.
Diterbitkan untuk:Schneider Electric Indonesia
Lampiran
Jelajahi lebih lanjut
Jelajahi lebih lanjut