Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
Negative Power Flow and Readings for kW, kVAR, and kWh

Product Line
CM4000 series
CM3000 series
CM2000 series
CM100/200 series
PM800

Environment
Measurements

Resolution
The only two readings that will change with negative powerflow are kW and kVAR. kWh will change only if the Circuit Monitor is in Signed mode. The default mode for the Circuit Monitors is Absolute mode.

Note: ION Meters only have Absolute mode.