FAQ Pencarian
How do I apply remote CJC to the BMXART0814 module?
Most end users choose to use the ABE7 CPA412 Telefast blocks with the BMXART0814 module because the CJC compensation is done automatically. However in some cases the
end user may choose to use an external pT 100 RTD rather than the Telefast block. If you choose to add the pt 100 externally it would be wired as follows.
The pT100 would be wired to Channel 4, EX+ and EX- terminals
In the Module configuration screen select the following
Temperature from Ch 4-7 bloc
External pT100
50Hz
R-3162018
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: