FAQ Pencarian
Does the ATV312 have a run time or elapsed time meter?
Issue:
Run time on ATV312
Product Line:
Altivar 312
Environment:
All models
Cause:
None
Resolution:
Yes, parameter rtH (Operating time) in the SUP menu displays the total time that the motor has been powered up. If desired, this can be set as the default display. This operating time can be reset to zero by setting rPr = rtH in the FLt menu.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Kategori:
Jelajahi lebih lanjut
Kategori: