Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
How is the Start/Stop circuit wired for the ATS48 soft starter?
Issue:
Where do you wire the start run circuit for the ATS48 soft starter?

Product Line:
Altistart 48 ATS48

Environment:
All

Cause:
NA

Resolution:
For 2-wire control , jumper the RUN and STOP terminals and wire a run contact between the 24V and RUN terminals.
2 wire control
For 3-wire control, wire a N/C stop contact between 24V and STOP and wire a N/O start contact between 24V and RUN.
3 wire control