Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
How to increase the drive size of VMware Image?

Issue
How to increase the drive size of VMware Image?

Product Line
VMware

Environment
VMware

Cause
Original size of Operating System C: drive is 40GB and now require to increase the size to 60GB

Resolution

1) Visit https://www.vmware.com/ and download VMware vCenter Converter Standalone
2) From
VMware vCenter Converter Standalone file menu select New -> Convert machine
3)  Leave the Select source type: VMware Workstation or other VMware virtual machine selected in the drop-down
and use the Browse button to select the  source image to convert, and click on the Next button
4) Select the location for the new VMware image
5) In the next window, the Options of the new image can be configured by clicking on the Edit button
How to increase the drive size of VMware Image
6) From the Data copy type drop down select "Select volumes to copy."

7) Here in the Designation size select and enter the new value
How to increase the drive size of VMware Image
8) Review the Summary in the next page and click on the Finish button