FAQ Pencarian
How to retrieve Sepam 2000 lost password?
If you forget or lose the password of Sepam 2000. You can acquire the password by using two solutions.
You will find attached a zip file with two files inside:
One file is a PowerPoint file explaining how to retrieve Sepam 2000 password using a PER2901 connected to COM1 of a PC. The other file is an exe file to read Sepam memory cartridge and then retrieve Sepam 2000 password. This exe file works on Windows XP and Windows 7 if PER2901 is connected to COM1 port.
You will find attached a zip file with two files inside:
One file is a PowerPoint file explaining how to retrieve Sepam 2000 password using a PER2901 connected to COM1 of a PC. The other file is an exe file to read Sepam memory cartridge and then retrieve Sepam 2000 password. This exe file works on Windows XP and Windows 7 if PER2901 is connected to COM1 port.
Diterbitkan untuk:Schneider Electric Indonesia
Lampiran
Jelajahi lebih lanjut
Jelajahi lebih lanjut