Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
Is the remote keypad cable a straight through CAT5 cable, referenced in part numbers VW3A1104R10 through R100?
Issue:
Remote keypad cable a straight through CAT5 cable, referenced in part numbers VW3A1104R10 through R100

Product Line:
ATV61 ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
Yes, the VW3A1104R10 through R100 is a straight through CAT 5 cable.