Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
What are the causes and remedy for Err8 fault on the ATV212 or SFD212 drives?
Issue:
ATV212 or SFD212 is showing ERR8 fault code.

Product Line:
Altivar ATV21, ATV212 SFD21 and SFD212 drives

Environment:
All

Cause:
Loss of network or network timeout has occurred.

Resolution:
Err8 means network communication fault error. Try checking the network control devices and cables.
The function can be disabled temporarily for troubleshooting by setting F803 to 0 and F851 to 1. However, please do not leave the network disabled. Once troubleshooting is over, please enable F803 back to 1 and F851 back to 4.