FAQ Pencarian
SoMachine Basic: How can I insert a Free POU between two Free POUs
The option menu "Insert Free POU" is not yet available in SoMBasic v1.4
If you want to insert a Free POU in the middle of two others, you can follow these steps:
If you want to insert a Free POU in the middle of two others, you can follow these steps:
- Add a new free POU
- Select the new free POU
- Use the keyboard CTRL+X (cut)
- Select the Free POU where you want to insert the new free POU
- now use the keyboard Ctrl+V (paste)
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: