Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
What analog inputs are available on the ATV630 Process Drive?

Article available in these languages: Spanyol

Issue:
ATV630 process drive analog inputs available.

Product line:
Altivar Process, ATV630, ATV600, Altivar 630

Environment:
All serial numbers

Cause:
n/a

Resolution:
The ATV630 drive comes with three analog inputs.  Each is programmable to be used for voltage or current.

The Min and Max Values are independently adjustable to allow setting up as voltage or current speed reference for most applications.  For example, 0-10V, 2-10V, 4-20mA, 20-0mA, etc.

Schneider Electric Indonesia

Lampiran
ATV600 analog inputs.jpg [36.7 KB]